Veuillez noter qu'Internet Explorer ne sera plus pris en charge après le 16 mai 2022. Nous vous recommandons de passer à Microsoft Edge ou Chrome.
Synchronisation en coursLes données de votre compte sont en cours de synchronisation.Les données de votre compte sont en cours de synchronisation.Les données de votre compte sont en cours de synchronisation.
Read this documentation before initial operation or use. This is a prerequisite for safe, trouble-free handling and use of the product.
Observe the safety instructions and warnings in this documentation and on the product.
Always keep the operating instructions with the product and make sure that the operating instructions are with the product when it is given to other persons.
Explanation of symbols
Warnings
Warnings alert you to hazards that can occur when you are handling or using the product. The following signal words are used in combination with a symbol:
DANGER! Draws attention to imminent danger leading to serious injury or fatality.
WARNING! Draws attention to a potential threat of danger that can lead to serious injury or fatality.
CAUTION! Draws attention to a potentially dangerous situation that can lead to minor injury or damage to the equipment or other property
Symbols in the documentation
The following symbols are used in this document:
Read the operating instructions before use
Instructions for use and other useful information
Dealing with recyclable materials
Do not dispose of electric equipment as household waste
Symbols in the illustrations
The following symbols are used in illustrations:
These numbers refer to the corresponding illustrations found at the beginning of these operating instructions
The numbering reflects the sequence of operations shown in the illustrations and may deviate from the steps described in the text
Item reference numbers are used in the overview illustrations and refer to the numbers used in the product overview section
This symbol is intended to draw special attention to certain points when handling the product.
Wireless data transfer
Product-dependent symbols
Symbols on the product
The following symbols are used on the product:
Wear eye protection.
Revolutions per minute
Revolutions per minute
Rated speed
Diameter
Protection class II (double-insulated)
Product information
Hilti products are designed for professional use and may be operated, serviced and maintained only by trained, authorized personnel. This personnel must be informed of any particular hazards that may be encountered. The product described and its ancillary equipment may present hazards when used incorrectly by untrained personnel or when used not as directed.
The type designation and serial number are printed on the rating plate.
Write down the serial number in the table below. Always quote this information when you contact a Hilti representative or Hilti Service to enquire about the product. Product information
Product information
Angle grinder
AG 125-13S
Generation
05
Serial no.
Declaration of conformity
We declare, on our sole responsibility, that the product described here complies with the applicable directives and standards. A copy of the declaration of conformity can be found at the end of this documentation.
The technical documentation is filed here:
Hilti Entwicklungsgesellschaft mbH | Tool Certification | Hiltistrasse 6 | 86916 Kaufering, Germany
Safety
General power tool safety warnings
WARNING
Read all safety warnings and all instructions. Failure to follow the warnings and instructions may result in electric shock, fire and/or serious injury.
Save all warnings and instructions for future reference. Work area safety
Keep work area clean and well lit. Cluttered or dark areas invite accidents.
Do not operate power tools in explosive atmospheres, such as in the presence of flammable liquids, gases or dust. Power tools create sparks which may ignite the dust or fumes.
Keep children and bystanders away while operating a power tool. Distractions can cause you to lose control.
Electrical safety
Power tool plugs must match the outlet. Never modify the plug in any way. Do not use any adapter plugs with earthed (grounded) power tools. Unmodified plugs and matching outlets will reduce risk of electric shock.
Avoid body contact with earthed or grounded surfaces, such as pipes, radiators, ranges and refrigerators. There is an increased risk of electric shock if your body is earthed or grounded.
Do not expose power tools to rain or wet conditions. Water entering a power tool will increase the risk of electric shock.
Do not abuse the cord. Never use the cord for carrying, pulling or unplugging the power tool. Keep cord away from heat, oil, sharp edges or moving parts. Damaged or entangled cords increase the risk of electric shock.
When operating a power tool outdoors, use an extension cord suitable for outdoor use. Use of a cord suitable for outdoor use reduces the risk of electric shock.
If operating a power tool in a damp location is unavoidable, use a residual current device (RCD) protected supply. Use of an RCD reduces the risk of electric shock.
Personal safety
Stay alert, watch what you are doing and use common sense when operating a power tool. Do not use a power tool while you are tired or under the influence of drugs, alcohol or medication. A moment of inattention while operating power tools may result in serious personal injury.
Use personal protective equipment. Always wear eye protection. Protective equipment such as dust mask, non-skid safety shoes, hard hat, or hearing protection used for appropriate conditions will reduce personal injuries.
Prevent unintentional starting. Ensure the switch is in the off‐position before connecting to power source, picking up or carrying the tool. Carrying power tools with your finger on the switch or energising power tools that have the switch on invites accidents.
Remove any adjusting key or wrench before turning the power tool on. A wrench or a key left attached to a rotating part of the power tool may result in personal injury.
Do not overreach. Keep proper footing and balance at all times. This enables better control of the power tool in unexpected situations.
Dress properly. Do not wear loose clothing or jewellery. Keep your hair, clothing and gloves away from moving parts. Loose clothes, jewellery or long hair can be caught in moving parts.
If devices are provided for the connection of dust extraction and collection facilities, ensure these are connected and properly used. Use of dust collection can reduce dust-related hazards.
Power tool use and care
Do not force the power tool. Use the correct power tool for your application. The correct power tool will do the job better and safer at the rate for which it was designed.
Do not use the power tool if the switch does not turn it on and off. Any power tool that cannot be controlled with the switch is dangerous and must be repaired.
Disconnect the plug from the power source from the power tool before making any adjustments, changing accessories, or storing power tools. Such preventive safety measures reduce the risk of starting the power tool accidentally.
Store idle power tools out of the reach of children and do not allow persons unfamiliar with the power tool or these instructions to operate the power tool. Power tools are dangerous in the hands of untrained users.
Maintain power tools. Check for misalignment or binding of moving parts, breakage of parts and any other condition that may affect the power tool’s operation. If damaged, have the power tool repaired before use. Many accidents are caused by poorly maintained power tools.
Keep cutting tools sharp and clean. Properly maintained cutting tools with sharp cutting edges are less likely to bind and are easier to control.
Use the power tool, accessories and tool bits etc. in accordance with these instructions, taking into account the working conditions and the work to be performed. Use of the power tool for operations different from those intended could result in a hazardous situation.
Service
Have your power tool serviced by a qualified repair person using only identical replacement parts. This will ensure that the safety of the power tool is maintained.
Safety warnings common for grinding, sanding, wire brushing, polishing or abrasive cutting-off operations:
This power tool is intended to function as a grinder, sander, wire brush or cut-off tool. Read all safety warnings, instructions, illustrations and specifications provided with this power tool. Failure to follow all instructions listed below may result in electric shock, fire and/or serious injury.
Operations such as polishing are not recommended to be performed with this power tool. Operations for which the power tool was not designed may create a hazard and cause personal injury.
Do not use accessories which are not specifically designed and recommended by the tool manufacturer. Just because the accessory can be attached to your power tool, it does not assure safe operation.
The rated speed of the accessory must be at least equal to the maximum speed marked on the power tool. Accessories running faster than their rated speed can break and fly apart.
The outside diameter and the thickness of your accessory must be within the capacity rating of your power tool. Incorrectly sized accessories cannot be adequately guarded or controlled.
Threaded mounting of accessories must match the grinder spindle thread. For accessories mounted by flanges, the arbour hole of the accessory must fit the locating diameter of the flange. Accessories that do not match the mounting hardware of the power tool will run out of balance, vibrate excessively and may cause loss of control.
Do not use a damaged accessory. Before each use inspect the accessory such as abrasive wheels for chips and cracks, backing pad for cracks, tear or excess wear, wire brush for loose or cracked wires. If power tool or accessory is dropped, inspect for damage or install an undamaged accessory. After inspecting and installing an accessory, position yourself and bystanders away from the plane of the rotating accessory and run the power tool at maximum no-load speed for one minute. Damaged accessories will normally break apart during this test time.
Wear personal protective equipment. Depending on application, use face shield, safety goggles or safety glasses. As appropriate, wear dust mask, hearing protectors, gloves and workshop apron capable of stopping small abrasive or workpiece fragments. The eye protection must be capable of stopping flying debris generated by various operations. The dust mask or respirator must be capable of filtrating particles generated by your operation. Prolonged exposure to high intensity noise may cause hearing loss.
Keep bystanders a safe distance away from work area. Anyone entering the work area must wear personal protective equipment. Fragments of workpiece or of a broken accessory may fly away and cause injury beyond immediate area of operation.
Hold the power tool by insulated gripping surfaces only, when performing an operation where the cutting accessory may contact hidden wiring or its own cord. Cutting accessory contacting a "live" wire may make exposed metal parts of the power tool "live" and could give the operator an electric shock.
Position the cord clear of the spinning accessory. If you lose control, the cord may be cut or snagged and your hand or arm may be pulled into the spinning accessory.
Never lay the power tool down until the accessory has come to a complete stop. The spinning accessory may grab the surface and pull the power tool out of your control.
Do not run the power tool while carrying it at your side. Accidental contact with the spinning accessory could snag your clothing, pulling the accessory into your body.
Regularly clean the power tool’s air vents. The motor’s fan will draw the dust inside the housing and excessive accumulation of powdered metal may cause electrical hazards.
Do not operate the power tool near flammable materials. Sparks could ignite these materials.
Do not use accessories that require liquid coolants. Using water or other liquid coolants may result in electrocution or shock.
Kickback and related warningsKickback is a sudden reaction to a pinched or snagged rotating wheel, backing pad, brush or any other accessory. Pinching or snagging causes rapid stalling of the rotating accessory which in turn causes the uncontrolled power tool to be forced in the direction opposite of the accessory’s rotation at the point of the binding.
For example, if an abrasive wheel is snagged or pinched by the workpiece, the edge of the wheel that is entering into the pinch point can dig into the surface of the material causing the wheel to climb out or kick out. The wheel may either jump toward or away from the operator, depending on direction of the wheel’s movement at the point of pinching. Abrasive wheels may also break under these conditions.
Kickback is the result of power tool misuse and/or incorrect operating procedures or conditions and can be avoided by taking proper precautions as given below.
Maintain a firm grip on the power tool and position your body and arm to allow you to resist kickback forces. Always use auxiliary handle, if provided, for maximum control over kickback or torque reaction during start-up. The operator can control torque reactions or kickback forces, if proper precautions are taken.
Never place your hand near the rotating accessory. Accessory may kickback over your hand.
Do not position your body in the area where power tool will move if kickback occurs. Kickback will propel the tool in direction opposite to the wheel’s movement at the point of snagging.
Use special care when working corners, sharp edges etc. Avoid bouncing and snagging the accessory. Corners, sharp edges or bouncing have a tendency to snag the rotating accessory and cause loss of control or kickback.
Do not attach a saw chain woodcarving blade or toothed saw blade. Such blades create frequent kickback and loss of control.
Safety warnings specific for grinding and abrasive cutting-off operations:
Use only wheel types that are recommended for your power tool and the specific guard designed for the selected wheel. Wheels for which the power tool was not designed cannot be adequately guarded and are unsafe.
The grinding surface of centre depressed wheels must be mounted below the plane of the guard lip. An improperly mounted wheel that projects through the plane of the guard lip cannot be adequately protected.
The guard must be securely attached to the power tool and positioned for maximum safety, so the least amount of wheel is exposed towards the operator. The guard helps to protect the operator from broken wheel fragments, accidental contact with wheel and sparks that could ignite clothing.
Wheels must be used only for recommended applications. For example: do not grind with the side of cut-off wheel. Abrasive cut-off wheels are intended for peripheral grinding, side forces applied to these wheels may cause them to shatter.
Always use undamaged wheel flanges that are of correct size and shape for your selected wheel . Proper wheel flanges support the wheel thus reducing the possibility of wheel breakage. Flanges for cut-off wheels may be different from grinding wheel flanges.
Do not use worn down wheels from larger power tools. Wheel intended for larger power tool is not suitable for the higher speed of a smaller tool and may burst.
Additional safety warnings specific for abrasive cutting-off operations:
Do not "jam" the cut-off wheel or apply excessive pressure. Do not attempt to make an excessive depth of cut. Overstressing the wheel increases the loading and susceptibility to twisting or binding of the wheel in the cut and the possibility of kickback or wheel breakage.
Do not position your body in line with and behind the rotating wheel. When the wheel, at the point of operation, is moving away from your body, the possible kickback may propel the spinning wheel and the power tool directly at you.
When wheel is binding or when interrupting a cut for any reason, switch off the power tool and hold the power tool motionless until the wheel comes to a complete stop. Never attempt to remove the cut-off wheel from the cut while the wheel is in motion otherwise kickback may occur. Investigate and take corrective action to eliminate the cause of wheel binding.
Do not restart the cutting operation in the workpiece. Let the wheel reach full speed and carefully re-enter the cut. The wheel may bind, walk up or kickback if the power tool is restarted in the workpiece.
Support panels or any oversized workpiece to minimize the risk of wheel pinching and kickback. Large workpieces tend to sag under their own weight. Supports must be placed under the workpiece near the line of cut and near the edge of the workpiece on both sides of the wheel.
Use extra caution when making a "pocket cut" into existing walls or other blind areas. The protruding wheel may cut gas or water pipes, electrical wiring or objects that can cause kickback.
Safety warnings specific for sanding operations:
Do not use excessively oversized sanding disc paper. Follow manufacturers recommendations, when selecting sanding paper. Larger sanding paper extending beyond the sanding pad presents a laceration hazard and may cause snagging, tearing of the disc or kickback.
Safety warnings specific for wire brushing operations:
Be aware that wire bristles are thrown by the brush even during ordinary operation. Do not overstress the wires by applying excessive load to the brush. The wire bristles can easily penetrate light clothing and/or skin.
If the use of a guard is recommended for wire brushing, do not allow any interference of the wire wheel or brush with the guard. Wire wheel or brush may expand in diameter due to work load and centrifugal forces.
Additional safety instructions
Personal safety
Use the product only when it is in technically faultless condition.
Never tamper with or modify the tool in any way.
Always hold the power tool with both hands on the handles provided. Keep the handles clean and dry.
Avoid touching rotating parts – risk of injury!
Wear suitable protective glasses, a hard hat, ear protection, protective gloves and light respiratory protection while using the power tool.
Before beginning the work, check the hazard classification of the dust that will be produced. Use an industrial vacuum cleaner with an officially approved protection class in compliance with the locally applicable dust protection regulations. Dust from materials such as lead-based paint, certain types of wood and concrete/masonry/stone containing quartz, minerals or metal may be harmful to health.
Make sure that the workplace is well ventilated and, where necessary, wear a respirator appropriate for the type of dust generated. Contact with or inhalation of the dust may cause allergic reactions and/or respiratory or other diseases among operators or bystanders. Certain kinds of dust are classified as carcinogenic such as oak and beech dust, especially in conjunction with additives for wood conditioning (chromate, wood preservative). Material containing asbestos may be handled only by specialists.
Take breaks between working and do physical exercises to improve the blood circulation in your fingers. Exposure to vibration during long periods of work can lead to disorders of the blood vessels and nervous system in the fingers, hands and wrists.
Electrical safety
Before beginning work, check the working area for concealed electric cables or gas and water pipes. External metal parts of the power tool may give you an electric shock if you damage an electric cable accidentally.
Do not touch the supply cord or extension cord if it is damaged while working. Disconnect the mains plug from the power outlet. Check the tool’s supply cord at regular intervals and have it replaced by Hilti Service if damage is found. Check extension cords at regular intervals and replace them if found to be damaged.
Using and handling power tools with care
Do not use cutting discs for grinding.
Remove the clamping flange from the arbor before fitting a threaded accessory tool.
Tighten the accessory tool and flange securely. If the accessory tool and flange are not tightened securely, the accessory tool may work loose from the arbor due to the braking effect of the motor after switching off.
Comply with the manufacturer's instructions for handling and storing grinding discs.
Description
Overview of the product
Spindle lockbutton
On/off switch
Air vents
Vibration-absorbing side handle
Wrench
Clamping nut
Kwik lock clamping nut (optional)
Cutting disc / grinding disc
Clamping flange with O-ring
Guard
Spindle
Quick locking system
Guard release button
Threaded bushing for handle
Intended use
The product described is a hand-held electric angle grinder. It is designed for cutting and grinding metal and mineral materials, and for brushing, sanding and drilling in tiles, all without use of water. It may used only for dry cutting / grinding.
The tool may be operated only when connected to a power supply providing a voltage and frequency in compliance with the information given on its rating plate.
The power tool may be used for cutting, slitting and grinding mineral materials only when equipped with the corresponding guard and front cover.
A dust removal hood together with a suitable Hilti vacuum cleaner must be used for working on mineral materials such as concrete or stone.
Items supplied
Angle grinder, side handle, standard guard, front cover, clamping flange, clamping nut, wrench, operating instructions.
Other system products approved for use with this product can be found at your local
Hilti Store or at:
www.hilti.group | USA:
www.hilti.com
Starting current limiter
The electronic starting current limiter reduces the starting current drawn to prevent the line fuse from tripping. This prevents abrupt start-up of the product.
Constant-speed electronics
Electronic speed control keeps running speed almost constant irrespective of whether the power tool is idling or running under load. Constant running speed helps ensure maximum efficiency.
Active Torque Control (ATC)
The electronics detect potential stalling of the disc and prevent further rotation of the arbor by switching off the product.
If the ATC system has been triggered, restart the product. Do this by releasing the on/off switch and then pressing it again.
If the ATC system fails, the product will run at greatly reduced speed and with greatly reduced torque. Have the product checked by
Hilti Service.
Restart interlock
The product does not restart by itself when the on/off switch is locked in the ON position and power is restored after an interruption in the electric supply. The on/off switch must first be released and then pressed again.
Temperature-dependent product protection
The temperature-dependent motor protection system monitors current input and motor temperature and thus prevents the power tool overheating.
If the motor is overloaded through application of excessive working pressure, the product’s performance drops noticeably or it might stall completely. A standstill should be avoided. No specific value can be given for the permissible overloading limit for the power tool as it depends on motor temperature.
Front cover for the disc guard
When grinding with straight grinding discs and cutting with cutting discs in metalworking applications, use the standard guard with front cover.
DG-EX 125/5" dust hood for grinding (accessory)
The grinding system is suitable only for occasional use with diamond cup wheels for grinding mineral materials.
CAUTION Use of this hood for working on metal is prohibited.
DC-EX 125/5"M dust hood for grinding (accessory)
The power tool may be used for cutting and slitting work on mineral materials only when fitted with a dust hood.
CAUTION Use of this hood for working on metal is prohibited.
DC-EX 125/5"C dust hood for cutting (accessory)
Use the DC-EX 125/5"C dust hood when cutting masonry and concrete.
CAUTION Use of this hood for working on metal is prohibited.
Consumables
Only synthetic resin-bonded, fiber-reinforced discs with a maximum diameter of Ø 125 mm which are approved for use at a rotational speed of at least 11,500/min and a peripheral speed of 80 m/s may be used.
The maximum grinding disc thickness is 6.4 mm and the maximum cutting disc thickness is 2.5 mm.
WARNING! When cutting or slitting with cutting discs, always use the standard guard with additional cover plate. Discs
Application
Designation
Material
Abrasive cutting disc
Cutting, slitting
AC‑D
Metal
Diamond cutting disc
Cutting, slitting
DC-TP, DC-D (SPX, SP, P)
Mineral
Abrasive grinding disc
Rough grinding
AG‑D, AF‑D, AN‑D
Metal
Diamond grinding disc
Rough grinding
DG-CW (SPX, SP, P)
Mineral
Wire brushes
Wire brushes
3CS, 4CS, 3SS, 4SS
Metal
Diamond core bit
Drilling in tiles
DD-M14
Mineral
Abrasive resin-fiber disc
Rough grinding
AP-D
Metal
Suitability of discs for the equipment used
Item
Equipment
AC‑D
AG‑D, AF‑D, AN‑D
DG-CW (SPX, SP, P)
DC-TP, DC-D (SPX, SP, P)
AP-D
3CS, 4CS, 3SS, 4SS, DD-M14
A
Guard
X
X
X
X
X
X
B
Front cover (in combination with A)
X
—
—
X
—
—
C
DG-EX 125/5" dust hood for grinding
—
—
X
—
—
—
D
DC-EX 125/5"C dust hood for cutting (only in conjunction with A)
—
—
—
X
—
—
E
DC-EX 125/5"M dust hood for slitting
—
—
—
X
—
—
F
DC‑EX SL adapter (in conjunction with E)
—
—
—
X
—
—
G
Side handle
X
X
X
X
X
X
H
DCBG 125 hoop handle (optional for G)
X
X
X
X
X
X
I
Clamping nut
X
X
X
X
—
—
J
Clamping flange
X
X
X
X
—
—
K
Kwik lock (optional for I)
X
—
—
X
—
—
L
Clamping nut for abrasive resin-fiber disc
—
—
—
—
X
—
M
Support plate
—
—
—
—
X
—
Technical data
Angle grinder
If the product is powered by a generator or transformer, the generator or transformer’s power output must be at least twice the rated input power shown on the rating plate of the product. The operating voltage of the transformer or generator must always be within +5 % and -15 % of the rated voltage of the product.
The information given applies for a rated voltage of 230 V. Actual figures can vary for country-specific versions and if the voltage supply differs. For rated voltage, frequency, input power and rated current, refer to the rating plate.
AG 125-13S
Rated power input
1,300 W
Rated speed
11,500 /min
Maximum disc diameter
125 mm
Thread diameter
M14
Thread length
22 mm
Weight in accordance with EPTA procedure 01
2.5 kg
Noise information and vibration values in accordance with EN 60745
The sound pressure and vibration values given in these instructions were measured in accordance with a standardized test and can be used to compare one power tool with another. They can also be used for a preliminary assessment of exposure. The data given represents the main applications of the power tool. However, if the power tool is used for different applications, with different accessory tools, or is poorly maintained, the data can vary. This can significantly increase exposure over the total working period. An accurate estimation of exposure should also take into account the times when the tool is switched off, or when it is running but not actually being used for a job. This can significantly reduce exposure over the total working period. Identify additional safety measures to protect the operator from the effects of noise and/or vibration, for example: Maintaining the power tool and accessory tools, keeping the hands warm, organization of work patterns.
Noise information
AG 125-13S
Sound (power) level (LWA)
102 dB(A)
Emission sound pressure level (LpA)
91 dB(A)
Uncertainty for the sound pressure level (KpA)
3 dB(A)
Vibration informationOther applications, such as cutting, may produce vibration values that deviate from the given values.
AG 125-13S
Surface grinding with the vibration-absorbing side handle (ah,AG)
5.3 m/s²
Sanding (ah,DS)
4.0 m/s²
Uncertainty (K)
1.5 m/s²
Before use
CAUTION
Risk of injury. The accessory tool may be hot or have sharp edges.
Wear protective gloves when fitting, removing or adjusting the accessory tool or other parts and when troubleshooting.
Fitting the side handle
Screw the side handle into one of the threaded bushings provided.
Guard
Observe the instructions for fitting the applicable guard.
Installing the guard
The guard is keyed to ensure that only guards of a type suitable for use with the product can be installed. The keyed locating lug also prevents the guard from coming into contact with the tool.
Fit the guard on to the arbor collar so that the two triangular marks on the guard and on the product are in alignment.
Press the guard on to the drive spindle collar.
Press the guard release button and turn the guard until it engages in the desired position.
The guard release button jumps back.
Adjusting the guard
Press the guard release button and then rotate the guard until it engages in the desired position.
Removing the guard
Press the guard release button and turn the guard until the triangular marks on the guard and on the product are in alignment.
Lift off the guard.
Fitting or removing the front cover
Position the front cover with the closed side on the standard guard and push it on until it engages.
To remove it, release the catch for the front cover and then lift the front cover away from the standard guard.
Fitting or removing the discs
CAUTION
Risk of injury. The accessory tool may be hot.
Wear protective gloves when changing the accessory tool.
Diamond discs must be replaced when their cutting or grinding performance drops significantly. This generally is the case when the diamond segments reach a height of less than 2 mm (1/16").
Other discs must be replaced when their cutting performance drops significantly or other parts of the angle grinder (not the disc) come into contact with the material you are working on.
Abrasive discs must be replaced when their expiry date has been reached.
Fitting the grinding disc
Disconnect the mains plug from the power outlet.
Check that the O-ring is in place in the clamping flange and that it is undamaged. Result The O-ring is damaged. There is no O-ring in the clamping flange.
Fit a new clamping flange with O-ring.
Fit the clamping flange onto the drive spindle.
Fit the grinding disc.
Screw on the clamping nut corresponding to the type of accessory tool fitted.
Press the spindle lockbutton and hold it in this position.
Use the pin wrench to tighten the clamping nut securely, then release the spindle lockbutton and remove the wrench.
Removing the grinding disc
Disconnect the mains plug from the power outlet.
CAUTION
Risk of breakage and irreparable damage. If the spindle lockbutton is pressed while the spindle is rotating, the accessory tool can detach from the power tool.
Press the spindle lockbutton only when the spindle has stopped rotating.
Press the spindle lockbutton and hold it in this position.
Release the clamping nut by gripping it with the pin wrench and turning the nut counterclockwise.
Release the spindle lockbutton and remove the grinding disc.
Fitting a grinding disc with a Kwik lock nut
CAUTION
Risk of breakage. Heavy wear (abrasion) may cause the
Kwik lock nut to break.
When working with the power tool, make sure that the Kwik lock nut doesn’t come into contact with the working surface.
Do not use a damaged Kwik lock nut.
The optional
Kwik lock nut can be used instead of the standard clamping nut. Grinding discs can then be changed without the need for additional tools.
Disconnect the supply cord plug from the power outlet.
Clean the clamping flange and the quick-release clamping nut.
Check that the O-ring is in place in the clamping flange and that it is undamaged. Result The O-ring is damaged. There is no O-ring in the clamping flange.
Fit a new clamping flange with O-ring.
Fit the clamping flange onto the drive spindle.
Fit the grinding disc.
Screw on the Kwik lock nut until it is seated against the grinding disc.
The name Kwik lock should be visible when the nut is screwed on.
Press the spindle lockbutton and hold it in this position.
Turn the grinding disc firmly by hand in a clockwise direction until the Kwik lock nut is tightened securely and then release the spindle lockbutton.
Removing a grinding disc secured with a Kwik lock nut
Disconnect the mains plug from the power outlet.
CAUTION
Risk of breakage and irreparable damage. If the spindle lockbutton is pressed while the spindle is rotating, the accessory tool can detach from the power tool.
Press the spindle lockbutton only when the spindle has stopped rotating.
Press the spindle lockbutton and hold it in this position.
Release the Kwik lock nut by turning it counterclockwise by hand.
If the Kwik lock nut cannot be released by turning it by hand, use a pin wrench to turn the nut in a counterclockwise direction.
Never use a pipe wrench! A pipe wrench could damage the
Kwik lock nut.
Release the spindle lockbutton and remove the grinding disc.
Fit the support plate and the abrasive resin-fiber disc, screw on the clamping nut and tighten it securely.
Press the spindle lockbutton and hold it in this position.
Use the pin wrench to tighten the clamping nut securely, then release the spindle lockbutton and remove the wrench.
Operation
Grinding
CAUTION
Risk of injury. The accessory tool may suddenly stick or stall.
Use the power tool with the side handle (or optional hoop grip) fitted and always hold the power tool securely with both hands.
Cutting
When cutting, apply moderate feed pressure and do not tilt the product or the cutting disc to either side (hold at approx. 90° to the cutting plane).
For best results when cutting profiles and small-section rectangular tubes, start cutting at the smallest cross section.
Rough grinding
Move the product to and fro while maintaining a 5° to 30° angle of attack and applying moderate pressure.
This will avoid overheating and discoloration of the workpiece and help ensure an even surface finish.
Switching on and off
Switching on
Plug the supply cord into the power outlet.
Press the rear section of the on/off switch.
Slide the on/off switch forward.
Lock the on/off switch.
The motor runs.
Switching off
Press the rear section of the on/off switch.
The on/off switch jumps into the off position and the motor stops.
Care of the product
DANGER
Electric shock due to breakdown of protective insulation. When working on metal under extreme conditions, conductive dust may accumulate inside the power tool, thereby adversely affecting the protective insulation.
Use a stationary dust extraction system when working under extreme conditions.
Clean the air vents frequently.
Use a ground fault circuit interrupter (PRCD) in the electric power supply line to the power tool.
WARNING
Electrical hazards. Improper repairs to electrical parts may lead to serious injuries.
Electrical parts may be repaired only by trained electrical specialists.
Never operate the product when the air vents are blocked. Clean the air vents carefully using a dry brush. Do not allow foreign objects to enter the interior of the product.
Keep the product, especially its grip surfaces, clean and free from oil and grease. Do not use cleaning agents containing silicone.
Clean the outside of the product at regular intervals using a slightly dampened cloth. Do not use a spray, steam pressure cleaning equipment or running water for cleaning.
Frequent work on conductive materials (e.g. metal, carbon fiber) may make shorter maintenance intervals necessary. Take your individual workplace risk assessment into account.
Checks after care and maintenance work
After carrying out care and maintenance, check that all protective and safety devices are fitted and that they function faultlessly.
Transport and storage
Do not transport the power tool with an accessory tool fitted to it.
Always unplug the supply cord before storing the power tool.
Store the product in a dry place where it cannot be accessed by children or unauthorized persons.
After long periods of transport or storage, check the power tool for damage before use.
Troubleshooting
If the trouble you are experiencing is not listed in this table or you are unable to remedy the problem by yourself, please contact
Hilti Service.
Troubleshooting
Trouble or fault
Possible cause
Action to be taken
Product does not start.
Interruption in the electric supply.
Plug in another power tool or appliance and check whether it works.
The supply cord or plug is defective.
Have the supply cord and plug checked by a trained electrical specialist and replaced if necessary.
The carbon brushes are worn.
Have the product checked by a trained electrical specialist; have the carbon brushes replaced, if necessary.
Product does not work.
Product is overloaded.
Release the on/off switch and then press it again. Then allow the product to run under no load for approx. 30 seconds.
Product does not develop full power.
The extension cord conductor cross section (gauge) is inadequate.
Use an extension cord with an adequate conductor cross section.
Elevated temperatures at the gear housing.
Short braking intervals.
Run the power tool under no load until it cools down.
Disposal
Most of the materials from which
Hilti tools and appliances are manufactured can be recycled. The materials must be correctly separated before they can be recycled. In many countries, your old tools, machines or appliances can be returned to
Hilti for recycling. Ask
Hilti Service or your Hilti representative for further information.
Do not dispose of power tools, electronic equipment or batteries as household waste!
RoHS (Restriction of Hazardous Substances)
The following links take you to the table of dangerous substances: qr.hilti.com/r4522554.
You will find a link to the RoHS table, in the form of a QR code, at the end of this document.
Manufacturer’s warranty
Please contact your local Hilti representative if you have questions about the warranty conditions.
Notre chat et le call back sont momentanément indisponibles mais nos points de vente ainsi que notre service client restent toujours disponibles par téléphone pour vous conseiller.
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
Heures d'ouverture du service clients : 8:00 - 18:00:
Etre rappelé(e) immédiatement par un conseiller
Etre rappelé(e) immédiatement par un conseiller
Indiquez-nous vos coordonnées et votre numéro de téléphone (sans espace entre les nombres), et nous vous rappellerons dans quelques minutes.
Le rappel automatique est disponible durant les heures d'ouverture : 9:00 - 17:00
Thank
You
Our executive will call you
back shortly
Chatter avec un conseiller
Chatter avec un conseiller
Chatter avec un conseiller
Nous envoyer un message
Nous envoyer un message
Envoyez-nous votre demande en remplissant ce formulaire.
Thank
You
An e-mail has been sent to our
Customer Service team for follow-up. You will receive a
copy of your request for your records.
Heures d'ouverture du service clients : 8:00 - 18:00:
Etre rappelé(e) immédiatement par un conseiller
Etre rappelé(e) immédiatement par un conseiller
Indiquez-nous vos coordonnées et votre numéro de téléphone (sans espace entre les nombres), et nous vous rappellerons dans quelques minutes.
Le rappel automatique est disponible durant les heures d'ouverture : 9:00 - 17:00
Thank
You
Our executive will
call you back shortly
Chatter avec un conseiller
Chatter avec un conseiller
Nous envoyer un message
Nous envoyer un message
Envoyez-nous votre demande en remplissant ce formulaire.
Thank
You
An e-mail has been sent to
our Customer Service team for follow-up. You will receive a
copy of your request for your records.